Other Parts Discussed in Thread: DLPC900, , DLP9000
Hi Team
This is a continuation of this Thread
The customer is planning on using TIDA-080008 to replace a RAPCUR era LED projector in order to use new generation LEDs. The projector uses the DLP9000 chipset with the DLPC900 control unit to control the LEDs - which per the user guide for your reference evaluation module uses 3.3V Enable and PMW signals to control the RAPCUR LED driver board in this instance. The customer wanted to make sure that the signals from the DLPC900 would indeed be able to control the TIDA-080008. Can you help confirm this?
I know that the RAPCUR module was an OSRAM product and not TIs, but since it was so commonly used in DLP LED projectors for years, I am hoping that the team has some experience with this and knows the pinouts for the LED driver control connectors on it.
I hope you can help.
Regards,
Marvin