The bqEVSW software (chip bq20z70) we are using now is connected with EV2300, which can export data in dfi format and gg format. But we need DFZX and xtx formats on our PCM, how do we convert them?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Xiaobo,
What are the DFZX and xtx formats? The golden image is an "image", which is stored in hex in the DFI format. You can refer the DFI documentation to convert to any format that you want. The gg format contains only settings and is not sufficient as a golden image.