This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am working with a multi channel 4-20mA input based on TIDA-00548. The differential inputs have a rather large offset compared to what a voltmeter indicates at the pins of the ADS1263 and as the differential voltage increases, the ADC value wraps from 00FFFFFF back to zero and then counts up without wrapping again. I have bypassed the PGA and am using the internal 2.5v reference, The 24.9 ohm burden resistor is raised above ground by the Schottky diode, just as in the reference design. The plus side of the resistor never exceeds 1.1 volts. This behavior is present on all boards tested. What could account for this behavior?
Hi Darryl,
thanks for contacting TI!
When bypassing the PGA there is a higher input current at the AIN signals (~150nA). The 4.99kOhm resistors may cause a drop seen in the result. If the input is open (no loop current). The offset can be automatically compensated by initializing the offset calibration registers.
Regarding 00FFFFFF is seems ADC2 (24bit is read) representing -1d in this case.
Hope this helps!
Best regards,
Lars
The apparent offset is 19 mV on top of the 13mV signal that I can measure with a DVM at the input pins. The 150nA input current does not account for this. With 13mV in, the reading is around D1DE23. I am not using the 24-bit ADC. After the reading overflows from 00FFFFFF to 0, and I continue to increase the input, the reading from the ADC reaches 043BCE39 at my full scale, which value is larger than 24 bits.
Hi Darryl,
Assuming you leave the input unconnected for the offset measurement the absolute voltage should be around 0V. This is ok regarding absolute input voltage range as you bypass the PGA.
D1DE23 equals to 16.012mV which is close to your DMM value (how accurate is you DMM at this low voltage?).
Are you measuring the 04BCE39 at ~3.3mA input current?
Can you explain more on the 00FFFFFF to 0 overflow? The only overflow should occur from FFFFFFFF to 0, i.e. -1 to 0.
The codes for the 24.9 shunt should linearly increase (ideally) from 5197A24 to 197F62B7 for the 4-20mA.
Best regards,
Lars
I have resolved the initial issue. In order to further characterize the problem I attempted to read back the register contents, and discovered that I could (no longer) read the factory default contents. I had to change the SPI configuration, and I should point out that for my TMS570LC4357 I had to set Polarity=1 and Phase=0 which is opposite of what the ADS1263 datasheet says. This change removed a mysterious 2X error in the resistance and voltage measurements as well as the odd overflow I saw in the differential measurements. My current measurements still have a 7uA offset (at zero current), that may be related to the 150nA input current you mentioned. In differential mode, would I see 150nA on each input or a total of 150nA ? How can I calculate the expected offset in the current measurement?
Hi Darryl,
good to hear you found the issue.
Data sheet mentions 350uV offset if chop mode is disabled. As you measure 7uA the corresponding voltage is 175uV, which is in the limits. Please try with chop mode enabled to compensate for the offset.
Best regards,
Lars
With PGA on and gain=1 the chop mode completely eliminated the differential mode offset. Thank you for the suggestion!