This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
Seeking on your assistance from Cx query.
With this post shared:
They are using PSpice tool and would like to import a .cir device from other manufacturer. After renaming the extension of the .cir file to .lib, the next step is associating a symbol. The free version of Pspice feature several libraries such as breakout.olb to pick a symbol from.
"Searching throughout alla the libraries though wasn't able to find a symbol which matches the SOIC-8. Figure out that I have to create one but the next question is: how can we do that? Where can I find the Symbol Editor?
Do I have to buy the full Pspice?"
For your assistance please.
Regards,
Archie A.
Hi Archie,
Please review the video mentioned in this post: (+) [FAQ] PSPICE-FOR-TI: How do I import a 3rd-party model into PSpice for TI? - Simulation, hardware & system design tools forum - Simulation, hardware & system design tools - TI E2E support forums
Thanks,
JC
Hello JC,
Thanks for replying, Cx responded:
Well, last reply didn't clear the last point we've ask for. It remains the following doubt: is there any "symbol editor"?
If I can't find any symbol in the libraries already installed which matches the pinout I have to create a suitable one.
The video you mentioned doesn't explain this point. If you can clear up this point would be great.
Thank you.
73,
Archie A.