Part Number: TIDA-01513
Hi All,
From the TIDA-01513, it mentioned that the basic or Reinforced isolation is used depends on peak voltage or voltage rating.
For normal 3 phase with 380VAC or 800VDC input for DC-DC side or HV battery, may I know how to judge which isolation shall we use?
Especially for below scenario,
1. 800V GND -> 12V GND
2. 800V GND -> Outer shell GND
Because we have to consider creepage distance so we want to figure out what kind of isolation we should use for above case.
And since we also recommend to use basic isolation between HV GND side and 12V GND then what scenario might not recommend to use basic isolation for same location?
Thank you.