Hi!
What's the purpose of L18-R85 in Control Pilot interface?
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jose,
I can help with explaining the purpose of L18 and R85 in the control pilot interface. The PLC and PWM parts of the CP have to be divided by a low pass filter. This filter circuit is described in the ISO15118-3:2015. The filter consists of an Inductor (typ. 220uH) and a damping resistor (typ. 220 Ohm) in parallel.
Best regards,
Errol
Ahhh. Ok. Thanks for the answer! But for only AC charging mode, without PLC is not necessary, is it?
Best regards!