My PSPICE for TI crashes every time when I start the simulation. I had our IT person to reinstall the program. Unfortunately, the issue continues. After the crash close the program, an error dialog appears followed by another dialog box, "This application has quit unexpectedly...". The first error dialog box shows
" INFO(ORNET-1112): PSpice Netlist Generation
INFO(ORNET-1059): Press cancel to quit
INFO(ORNET-1077): Creating header structure
Cancel "
I tried running my project on a different PC with PSpice for TI installed. The project ran fine on this other PC. I need to resolve this issue with my first PC. Help!
Note: The PC with the issue is an Windows 11 Pro (21H2 version), Intel I7 (12the Gen), 16 GB ram machine