This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP9204: Reference Design PMP9204

Part Number: PMP9204

Reference Design Number- PMP9204 (85-265) VAC

  1. Can This Power Supply working input  Voltage (75 to 275)VAC

What is min Ac Voltage is working with 1A Load

  1. I want to set output Voltage 5.1 or 5.2VDC. Which resistance value is change in Circuit?
  2. I want to set input under voltage and input over voltage limit. How will be set in circuit.
  3. Line and Load Variation
  4. I seen part number of transformer RLTI-1067 in BOM but there is no stock. Please suggest me any alternate part number of transformer.