Hi,
Customer would like to check the operation and behavior of this EVM board with DC input range from 300Vdc to 450Vdc for the server power aux application. Do you have any component change suggestion for the PMP21479 schematic to work with DC input from 300Vdc to 450Vdc and let this aux board operation normally? For example, change the C1 and C2 to the ones with 450Vdc rated cap. Don’t need to spend too much effort on efficiency improvement for this dc input range so far. Or do you have other aux EVM board suggestion for this dc input range operation? Thank you.

Best regards,
Randy