Hi Team,
Could you please help us to calculate the power dissipation for the below parts used in this reference design,
1.T2
2.Q10
3.Q11
4.Q6
5.Q8
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Could you please help us to calculate the power dissipation for the below parts used in this reference design,
1.T2
2.Q10
3.Q11
4.Q6
5.Q8
Hello Priyadharshini,
For the power dissipation of the transformer (T2) , we will need to contact the transformer vendor for more information about the core loss.
I will get back to you with a more definitive answer soon, along with the calculations for the FETs.
Thanks,
Sarah
Hi Priyadharshini,
You would need to contact the transformer vendor to find their core loss. This particular design uses 750318938 from Wurth Electronik.
FET power losses can be calculated with the following:
You may approximate FET losses by summing the switching, conduction (and gate drive) losses.
The FETs in this particular design do not have internal resistor, so you may neglect gate drive loss.
P_dissipated = P_sw + P_cond
P_sw = (E_on + E_off + E_rr) * f_sw
Values for the switching energies (E_on, E_off, E_rr) may be found in each FET's respective datasheet, however I believe some do not include this value.
In that case, you may estimate using:
E_oss = 0m5*C_oss*V_ds(off)^2
And then use 10*E_oss to approximate (E_on + E_off + E_rr)
f_sw is the switching frequency, typically 250 kHz
P_cond = I_rms^2 * R_ds(on)
Best,
Sarah