This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Import LT-Spice Models to PSpice for TI

I want to try different opamps to evaluate which one is best for my application (including TI opamps). As a base I need a component which is not available in the library of TI. I also looked on the PSpice page to see if the opamp is available:
www.pspice.com/.../all

In LT-Spice the component is available, and I can copy an AD8655.lib and an AD8655.asy. It should be possible to use these components in PSpice or? How do I set this up? I can create the component via Tool-Generate, but I get errors when simulating.

ERROR(ORPSIM-15108): Subcircuit AD8655 used by X_U5 is undefined

What am I doing wrong?

AD8655.lib