This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01505: How to change output voltage

Part Number: TIDA-01505
Other Parts Discussed in Thread: TL431-Q1

Hello everyone,

I am currently selecting a flyback converter for a traction inverter emergency supply.

I am happy with the voltage input range of TIDA-01505, but I would like an output of 10V with a current of up to 3.5A.

What do I need to change from the given design for the 15V output to achieve a 10V output? 

Thanks in advance and best regards

Til

  • Hi Til, the modification is very simple. As long as the transformer is able to support the required input voltage range, you need to just change the feedback divider such the FB_PSR stays 2.5V. Just change R78 or R28. I don't expect much effect to the loop compensation. For the optocoupler-based version, you need to change R73 or R69 around the TL431-Q1.

    This is a standard Flyback converter. You can learn more from the excellent PSDS seminar submission "Under the Hood of Flyback SMPS Designs"

    https://www.ti.com/seclit/ml/slup261/slup261.pdf

    I hope this helps. Best regards, Jiri