This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010232: AMC3330DWER & ADS131M06IPBS

Part Number: TIDA-010232
Other Parts Discussed in Thread: AMC3330,

Tool/software:

As per the reference design TIDA-010232 , We have designed an isolation monitoring circuit. But in our case Unlike the Reference design The AMC3330 amplified voltage  ±2.05-V (differential output signal) is provided to   ADS131M06IPBS(24 bit ADC). (AINXN - AINXP) . An external reference(1.25V) is provided to the 24 bit ADC. 

This would require modification in Calculation of  V Isolation Formula.(Provided in Design Guide - Equation 18)

Could you help us in the revised V isolation formula as per our use case ?

Also if you could share simulation file for the same.

Regards,

Kanhaiya Upreti

  • Hi Kanhaiya,

    In your case equation 18 would look like:

    Visolation =  VinADC* (RinAMC +Rst)/RinAMC *1/GainAMC

    You don't need VRef in the calculation since the ADS131 has a differential input and you will get a negative reading via SPI if there is a negative voltage on the input.

    Best regards,
    Andreas

  • Thanks for the update ,we will check and update you further. 

    We also have another Query regarding the Earth Loss Detection. In our circuit we have used two additional TPSI2140QDWQRQ1 (Switch) for adding a known resistance of 1.245 M ohm from DC+,DC- to earth.The RisoP ,RisoN equation will be now modified to Equation 21 & 22 (TIDA-010232). But what would be the accurate end result when earth is present and when its not present. Is there additional formula other then just calculating RisoP & RisoN (modified using Eq 21& 22). Also if you could provide any test example which help us understand the behavior under earth present and absent condition.

  • Hi Kanhaiya,

    Without the known resistor towards PE there is the problem, that you cant distinguish between a loss of PE and a really high insulation resistance, since in both cases the input voltage at the AMC3330 will be very low, ideally 0V. 

    If you add the known resistor towards PE the voltage at the input of AMC3330 is only 0 if PE is lost, otherwise you will measure the know resistance in parallel to RisoP/N, which will be always lower than the know resistance. 


    Best regards,

    Andreas

  • Hello Andreas ,

    Thanks for explanation of the behavior under Earth Present and absent condition, we will test and update you further on that . 

    Meanwhile, we are testing for isolation monitering in which we have used 2 switches only )

     we have calculated the RisoP & RisoN via the the method discussed before, and also used the modified equation you suggested for calculating VP ,VN

    (Visolation =  VinADC* (RinAMC +Rst)/RinAMC *1/GainAMC)

    We are following the software flow .

    1. Switch SP is closed and Vp is measured. You can use formula (18) on page 16 of the design guide to calculate the Isolation voltage which is Vp in case SP is closed
    2. Open SP , close SN, measured Vn, Again you can use formula (18) to calculate the Isolation voltage (In this case Vn)
    3. Calculate RisoP and RisoN using formulas (13) and (14)
    4. Check thresholds. If RisoP or RisoN is smaller then the fault threshold indicate a fault. If RisoP or RisoN is smaller than the warning threshold indicate a warning.

    one thing we observed that VinADC was having fluctuation , also sometimes the value was going in negative ,which would eventually effect Visolation, and RisoP & RisoN values. Please find the Excel attached. Can you confirm if the values & formula are okay .

    Regards isolation_check_pos.xlsx

    Kanhaiya

  • As per the design guide - 

    The original Equation 13 and Equation 14 for RisoN and RisoP are used now to calculate the parallel resistance of RisoP || RPE,P and RisoN || RPE,N. The values for RisoN and RisoP can be calculated by using Equation 21 and Equation 22.

    just to re confirm, we would close SP and close the switch for Additional Resistor (From Earth to Negative) together. Then we would calculate RisoN || RPE, using equation  13.

    Similarly  we would close SN and close the switch for Additional Resistor (From Earth to Positive) together. Then we would calculate RisoP || RPE, using equation  14.

    Then we need to use

     Equation 21 and Equation 22.

    RisoN and RisoP 

    Now the input of AMC3330 is only 0 if PE is lost, otherwise we will measure the known resistance in parallel to RisoP/N, which will be always lower than the know resistance. .

    Is our understanding correct ?

  • Hi Kanhaiya,

    Yes your procedure is correct, but negative input voltages on the ADC are not expected. 
    It should not be possible to get a negative input voltage at the ADC. It is possible however to have a negative voltage at the input of the isolated amplifier AMC3330, which is called VinAMC in the design guide.
    I suggest to start testing with known values for RisoP and RisoN and checking if the system is performing as expected.


    Best regards,

    Andreas

  •  . Can you suggest any other ways we can verify our results, also you said we can get negative voltage at the amc3330 input ,(VinAMC ). but then we are just feeding the same voltage to 24 bit ADC which is communicating with MCU. would it impact the risop and rison value. We are still using your suggested modified equation - 

    "Visolation =  VinADC* (RinAMC +Rst)/RinAMC *1/GainAMC

    You don't need VRef in the calculation since the ADS131 has a differential input and you will get a negative reading via SPI if there is a negative voltage on the input."

    Can you please provide us any method through which we can debug our issue and verify our test results ?

  • Hi Kanhaiya,

    Can you please describe the issue in more detail. Maybe a block diagram of your setup would help.
    The only way to verify results is by measuring the voltages at the different points of the system. 

    I also recommend to build a simple simulation of your file, then you can compare the results between the measurement and the simulation and find out where the root of the error is. 

    Best regards,
    Andreas

  • Hi Andreas ,

    Yes i am sharing a rough diagram(Attach with this message) to get you an idea of our setup , there is one modification though instead of  6.81k res , we are using 11 (33.2k ) resistors from DC+ to S1  (of first switch ),and also from  DC - to S2 (of Second switch ). 

    We will carry out the measurement , one more question ,in the first reply you said Quote "You don't need VRef in the calculation since the ADS131 has a differential input and you will get a negative reading via SPI if there is a negative voltage on the input." 

    So we would get a negative voltage ?  this negative voltage will be used in derivation of VIsolation

    becoz , (Visolation =  VinADC* (RinAMC +Rst)/RinAMC *1/GainAMC) ,

    and then RisoP/N. which would give us both -/+ resistance....?

    can you confirm  which values could be negative and which one should positive? 

    Regards,

    Kanhaiya 

    IsolationMonitering.pdf

  • Hi Kanhaiya,

    Thanks for sharing the diagram, this helps a lot.
    Yes you will get negative voltage but that's okay, this will not lead to a negative resistance, this will cancel out in the formulas for RisoN/P.

    Also for TIDA-010232 produces negative values for Visolation, since we subtract the reference voltage.

    Best regards,

    Andreas

  • Hi Andreas,

    we have measured the voltage via probing and through ADC, There is no discrepancy however we noticed that when the Switches (TPSI2140Q) are turned on ,right after that ,the reading of Vin P/N (voltage across sense resistor) is more but after 3-4 reads it stabilizes.(Reduced and gived stable and has less voltage value)

    i have prepared the excel sheet which contains manual calculator of RisoP & RisoN via the Formulas. (You can verify by providing the VINP/VInN values) and match with the Risop/n calculated via the ADC and compare with manual calculator.

    And it also contains the reading of VInP ,VinN , we got from ADC VIA MCU, and calculation of VP,VN, RisoP/N value done via the firmware.

    1. we are getting negative values as well as positive for VInP ,VinN. which is eventually giving us RIsoP & RisoN in negative sometimes.

    2. There is some discripancy between Value of RisoN Calculated via firmware and via Excel Calculator .

    why is that ? , our software flow is as following 

    1. we take 10 readings of VInP closing P Side switch and calculate Vp

    2. we take 10 reading of VInN closing N Side switch and calculate Vn

    3. We ignore the first 4 reading (we noticed that after 3-4 reads it stabilizes)

    4. then we take the Vp and Vn values from the above reading and calculate RisoP and RisoN 

    for eg - RisoP & RisoN considered taking 5th reading Vp and Vn values will be one reading.

    Can you please check the excel and our formula used in calculator , also please explain why we are getting negative resistance in calculator and also in ADC Calculation.Isolation Monitering Sheet.xlsx

    Waiting for your valuable reply 

    Thanks,

    Kanhaiya  

  • Hi Andreas ,

    We also tried one more exercise by connecting two100k one from DC- & one from DC+ to earth. Then we proceeded Measuring the RisoP & RisoN , but the values were no where near the 100K Values. (900k ) i have attached the sheet. Also when we removed earth still we were getting some resistance., but it was less then when the earth was present. (300k)

    Earth Detect.xlsx

  • Hi Andreas ,

    Any update on this above issue ? . we are still getting similar results after averaging the values  of Visolation and following the exact software flow with timing.

    attached files shows the result , still getting some negative resistances and also the RisoP & RisoN Values are different, deviation is too much in case of RisoN. Can you suggest any changes or issue with our formula or setup ?

     

    Isolation Monitering results (averaging).xlsx

  • Hi Kanhaiya,

    To be honest I am not sure at this moment what the issue is in your setup. 
    I think you need to debug this step by step. First lets do not use the Loss of PE circuit.

    From the excel sheet I see that you are using RstN/P = 365 kOhm and RinAMc = 294 Ohm.

    Please use two 100k resistors to simulate RisoP and RisoN.

    Then please just close SP:
    In this case the voltage at the input of AMC3330 should be 141 mV.
    The voltage at the ADC input should be 282 mV.


    Then open SP and close SN. In this case the input voltage at AMC3330 should be -141  mV
    The voltage at the ADC input should be -282 mV.

    Can you verify these voltages. 

    If you put this in your excel sheet the calculation works as expected and you get 100k for RisoN and RisoP.




    Best regards,

    Andreas

  • Hi Andreas ,

    We will try the above test you have recommended, externally using two 100k resistor connected from DC+ to Earth & DC- to earth. And then verify if we are getting the RisoP & RisoN value near to 100k

    . One doubt is that you have used the calculator sheet we have sent , and i can see RisoP & RisoN Coming around 109k & -109K .

    Is that correct value(not 100k)? also the resistance value is in negative is that ok ? . And do we expect same result via Firmware.

  • Hi Kanhaiya,


    This is because I did not put in all the decimals of vinAMCP and vinAMCN and i simulated for 400V and not for 402.77V.

    Also there is a mistake in the formula for RisoN. You need to divide by VP and not by VN. 
    So your formula shoudl be: =((B7+B6)*(B16+B18-B17))/B8

    Best regards,

    Andreas

  • Hi Andreas ,

    Thanks for the correction. we have revised the formula and yes now the resistance is in positive .We will retake the reading with External 100k Resistor to validate the Design. 

    Meanwhile could you provide your simulation file. Tina TI /PSPICE/LTSPICE any format will work .We would modify as per our design and validate.

    Regards

    Kanhaiya 

  • Full_AFE_SignalChain.TSC

    Hi Kanhaiya,

    Find the Tina Simulation attached.

    Best regards,

    Andreas

  • Hi Andreas ,

    Thanks for the simulation , we finally got our voltage same as the simulated circuit and we were able to get the 100k Value of RisoP & RisoN. Thanks for support .

    We are testing for Earth loss now. In our circuit we have two additional switches which basically add 1.245 M Ohm resistor from Earth to DC + and Earth to DC- . We turned those two switches ON and then Measured the RisoP & RisoN Values.

    Firmware Log are given Below When earth is present-  (using equation 13 and 14)

    Vdc: 402.817230, Vp: 74.473371, Vn: -74.576750, RisoP: 1243689.968640, RisoN: 1245416.375310

    As you can see we are getting values very close to the known resistor 1.245M Connected when earth is present .

    Now when we removed the earth the Value are changed , as given below - (using equation 13 and 14.)

    Vdc: 402.720520, Vp: 78.246364, Vn: -77.659671, RisoP: 1161596.654114, RisoN: 1152886.966650

    How can we know for sure that the earth is absent ?

    i would assume based on RisoP & RisoN Value?,

    1. when value is not near the known resistance , the earth is absent ?

    2. when value is near the known resistance , earth is present ?

    then we tried the formula given in the TIDA-010232, that states some modification in the RisoP & RisoN Formula, we  implemented that.

     Equation 21 & Equation 22. 

    But just to confirm our understanding .

    The  RisoP || RPE, RisoN || RPE, are the value which will be obtained using equation 13 and 14. right ?

    RPE,P & RNE,N will be 124500 Ohm(1.245Mohm) in our case ?

    then we calculate the RisoP & RisoN Using Eq 21 &  22.

    Please find the Firmware log for RisoP & RisoN values calculated via Eq 21 & 22 below ( when Earth is present)

    1. Vdc: 402.909180, Vp: 74.563210, Vn: -74.538084,

    RisoP: 1244535.065907, RisoN: 1244115.693987 (equation 13 and 14)

    earthRisop: 3332614619.412250 earthRisoN: 1751570176.805691  (Eq 21 & 22)

    2. Vdc: 402.854309, Vp: 74.474698, Vn: -74.635424,

    RisoP: 1242599.989988, RisoN: 1245281.682253 (equation 13 and 14)

    earthRisop: 644596055.826956 earthRisoN: -5503987846.279185  (Eq 21 & 22)

    Please find the Firmware log for RisoP & RisoN values calculated via Eq 21 & 22 below (when Earth is absent)

    1. Vdc: 402.939453, Vp: 77.862760, Vn: -77.973862,

    RisoP: 1158267.654711, RisoN: 1159920.379793 (equation 13 and 14)

    earthRisop: 16626360.388558 earthRisoN: 16973522.793565 (Eq 21 & 22)

    2  Vdc: 402.849060, Vp: 78.513005, Vn: -78.400813,

    RisoP: 1146516.876077, RisoN: 1144878.554049 (equation 13 and 14)

    earthRisop: 14493990.988998 earthRisoN: 14236448.407788 (Eq 21 & 22)

    In the above test also we are unable to get a conclusion on what basis should we consider that earth is absent or present?

    Regards

    Kanhaiya

  • Hi Andreas ,

    Any update on the above issue ? 

  • Hi Kanhaiya,

    Loss of earth can be detected if the measured value which is R_PE_N/P || RisoN/P is much bigger than the known resistor R_PE_N/P, since in a parallel connection its not possible that the parallel connection is bigger than one of the single resistors.

    Best regards,

    Andreas

  • hi Andreas ,

    We have measured the  R_PE_N/P || RisoN/P using equation 13 and 14 , with known resistance 1.245 M ohm, when earth is connected we are getting values closer to  1.245 M ohm. But when earth is Disconnected 1.12 M ohm. Which as per your statement is not accurate. "Loss of earth can be detected if the measured value which is R_PE_N/P || RisoN/P is much bigger than the known resistor R_PE_N/P".

    Can we connect on a call to have a short discussion ?

  • One more thing our earth and Digital GND is connected , will it impact the calculations ?

  • could you please provide your email address so we can connect ?

  • Hi Andreas ,

    Waiting for your response .

    Regards,

    Kanhaiya 

  • Hi Kanhaiya,

    What are the values for RisoN and RisoP in the test case when you have earth connected?

    Connecting digital GND and earth should not have a negative impact on the measurement, but it makes the isolation provided by AMC3330 and TPSI2140 obsolete. In that case a non isolated solution would perform better.

    Best regards,

    Andreas

  • Hi Andreas ,

    The values for RisoN and RisoP in our case is 1.245 Mohm, which we can enable via on Board additional switches.

    Our setup looks like the simulation Attached.

    Case 1.

    SPST1 & SPST2 were enabled and Earth was present .

    Then RisoP & RisoN was calculated via Eq 13 & 14 (On firmware)

    Results.

     Vdc: 402.909180,

      Vp: 74.563210,

     Vn: -74.538084,

    RisoP: 1244535.065907,

    RisoN: 1244115.693987 

    Case 2.

    SPST1 & SPST2 were enabled and Earth was absent .

    Then RisoP & RisoN was calculated via Eq 13 & 14 (On firmware)

    Results.

    Vdc: 402.939453

    Vp: 77.862760,

    Vn: -77.973862

    RisoP: 1158267.654711

    RisoN: 1159920.379793

     

    Note - we are turning on both the SPST1 & SPST2 Simultaneously then measuring the RisoP and RisoN under Earth Present and Absent condition.

    As you can see when earth is absent we are getting less resistance values of RisoP and RisoN (1.15Mohm) then the known Resistance 1.245 Mohm. 

    This shouldn't be the case as per your suggestion, it should be much higher then known resistance ?

    what do you recommend ?

    Isolation Monitering Updated.TSC 

  • Regarding Isolation Monitoring.

    Although we are getting Known Resistance when Connect known Resistance from Earth to DC+ & Earth to DC-. 

    But when we remove these known value , and calculate the actual RisoN & RisoP

    The values of RisoP & RisoN value seem to be increasing with time after turning on SP/SN.

    Please find the Log for Measured RisoP & RisoN Values below. This samples are captured at every 5ms interval. Please validate logs.
    Is there any timing limit that we need to consider samples till specific time after turn on SN/SP?

    -----------VP-----------------------------
    vdc, VinADC, VP
    
    
    Isolation : 402.741821,0.577111,358.725567
    Isolation : 402.712494,0.509821,316.898802
    Isolation : 402.834595,0.445570,276.961416
    Isolation : 402.784058,0.391628,243.431362
    Isolation : 402.761169,0.339546,211.058106
    Isolation : 402.818939,0.300888,187.028670
    Isolation : 402.858002,0.263702,163.913877
    Isolation : 402.848541,0.231420,143.847966
    Isolation : 402.797485,0.200120,124.392372
    Isolation : 402.791046,0.177902,110.581687
    Isolation : 402.797882,0.156804,97.467495
    Isolation : 402.806946,0.136903,85.097074
    Isolation : 402.883392,0.117711,73.167871
    Isolation : 402.813263,0.104934,65.225608
    Isolation : 402.880127,0.093368,58.036206
    Isolation : 402.800781,0.081272,50.517716
    Isolation : 402.786163,0.069237,43.036651
    Isolation : 402.831299,0.061932,38.495915
    Isolation : 402.913269,0.056161,34.909043
    Isolation : 402.904724,0.047613,29.595611
    Isolation : 402.881561,0.040016,24.873554
    Isolation : 402.807220,0.036261,22.539664
    Isolation : 402.880127,0.034119,21.207952
    Isolation : 402.835632,0.028544,17.742456
    Isolation : 402.891022,0.023576,14.654659
    Isolation : 402.868805,0.021728,13.505756
    Isolation : 402.845520,0.020718,12.878146
    Isolation : 402.828522,0.017174,10.675176
    Isolation : 402.834320,0.013034,8.101813
    Isolation : 402.844177,0.012853,7.989085
    Isolation : 402.797607,0.013164,8.182334
    Isolation : 402.862091,0.010558,6.562687
    Isolation : 402.814972,0.007449,4.629906
    Isolation : 402.847229,0.007448,4.629608
    Isolation : 402.863403,0.008700,5.408118
    Isolation : 402.858917,0.006492,4.035101
    Isolation : 402.851562,0.003408,2.118424
    Isolation : 402.912994,0.004349,2.703090
    Isolation : 402.835785,0.005609,3.486520
    Isolation : 402.803528,0.003786,2.353125
    Isolation : 402.903412,0.000889,0.552606
    Isolation : 402.871704,0.002419,1.503489
    Isolation : 402.852875,0.004123,2.562925
    Isolation : 402.872742,0.002599,1.615621
    Isolation : 402.937469,0.000498,0.309257
    Isolation : 402.876831,0.001278,0.794316
    Isolation : 402.818787,0.002649,1.646487
    Isolation : 402.788147,0.001640,1.019176
    Isolation : 402.879333,-0.000092,-0.057259
    Isolation : 402.914581,0.001318,0.819217
    Isolation : 402.884583,0.002750,1.709114
    Isolation : 402.819580,0.001407,0.874538
    Isolation : 402.887207,-0.000946,-0.588244
    Isolation : 402.948395,0.000233,0.145085
    Isolation : 402.879333,0.002210,1.373912
    Isolation : 402.823792,0.000954,0.593016
    Isolation : 402.854462,-0.001113,-0.692026
    Isolation : 402.911438,0.000142,0.088572
    Isolation : 402.843811,0.001832,1.138614
    Isolation : 402.823151,0.000736,0.457772
    Isolation : 402.895111,-0.000789,-0.490427
    Isolation : 402.859192,0.000337,0.209501
    Isolation : 402.894989,0.002273,1.412979
    Isolation : 402.897339,0.000237,0.147620
    Isolation : 402.828125,-0.001303,-0.809674
    Isolation : 402.801941,-0.000255,-0.158804
    Isolation : 402.896545,0.001649,1.024693
    Isolation : 402.918671,0.000346,0.215019
    Isolation : 402.861694,-0.001340,-0.832638
    Isolation : 402.821960,-0.000336,-0.208756
    Isolation : 402.829834,0.002047,1.272665
    Isolation : 402.886292,0.000611,0.379488
    Isolation : 402.963257,-0.000724,-0.450018
    Isolation : 402.895386,0.000022,0.013867
    Isolation : 402.844727,0.001885,1.171866
    Isolation : 402.768921,0.000723,0.449272
    Isolation : 402.827759,-0.001850,-1.149797
    Isolation : 402.929718,-0.000553,-0.343702
    Isolation : 402.951172,0.001389,0.863354
    Isolation : 402.841705,0.000332,0.206221
    Isolation : 402.808533,-0.001366,-0.849189
    Isolation : 402.871033,-0.000584,-0.363235
    Isolation : 402.858124,0.000832,0.517416
    Isolation : 402.819977,0.000549,0.341167
    Isolation : 402.879181,-0.001024,-0.636258
    Isolation : 402.838257,-0.000196,-0.121675
    Isolation : 402.911285,0.001181,0.734075
    Isolation : 402.797211,0.000141,0.087528
    Isolation : 402.852356,-0.001452,-0.902272
    Isolation : 402.839844,-0.000055,-0.034296
    Isolation : 402.853943,0.001943,1.207652
    Isolation : 402.832092,0.000441,0.274365
    Isolation : 402.883392,-0.001036,-0.644161
    Isolation : 402.858276,-0.000280,-0.174162
    Isolation : 402.788544,0.001725,1.071961
    Isolation : 402.830505,0.000562,0.349219
    Isolation : 402.844849,-0.000796,-0.494602
    Isolation : 402.819458,-0.000193,-0.119885
    Isolation : 402.896820,0.001631,1.013509
    Isolation : 402.860229,0.000611,0.380085
    Isolation : 402.821686,-0.001116,-0.693666
    Isolation : 402.861694,0.000250,0.155374
    Isolation : 402.871033,0.001787,1.110730
    Isolation : 402.943390,0.000615,0.382470
    Isolation : 402.930756,-0.000484,-0.300907
    Isolation : 402.904724,-0.000035,-0.021770
    Isolation : 402.842346,0.001638,1.018430
    Isolation : 402.765778,0.000787,0.489085
    Isolation : 402.861816,-0.001439,-0.894519
    Isolation : 402.947998,-0.000824,-0.512346
    Isolation : 402.900360,0.001411,0.877073
    Isolation : 402.840912,0.000500,0.310748
    Isolation : 402.895782,-0.001052,-0.654151
    Isolation : 402.860779,-0.000231,-0.143445
    Isolation : 402.929993,0.001500,0.932244
    Isolation : 402.864990,0.000671,0.417064
    Isolation : 402.816162,-0.001233,-0.766283
    Isolation : 402.954590,-0.000726,-0.451211
    Isolation : 402.919312,0.000905,0.562597
    Isolation : 402.866699,0.000401,0.249016
    Isolation : 402.805237,-0.001548,-0.961917
    Isolation : 402.909576,-0.000689,-0.428248
    Isolation : 402.974335,0.001279,0.795061
    Isolation : 402.902100,0.000458,0.284504
    Isolation : 402.803009,-0.001293,-0.803412
    Isolation : 402.881836,-0.000801,-0.497734
    Isolation : 402.872223,0.001012,0.629101
    Isolation : 402.868805,0.000821,0.510259
    Isolation : 402.836304,-0.000634,-0.393952
    Isolation : 402.825104,-0.000294,-0.182960
    Isolation : 402.875366,0.001673,1.039902
    Isolation : 402.894196,0.000154,0.095580
    Isolation : 402.841827,-0.001368,-0.850382
    Isolation : 402.842743,-0.000762,-0.473727
    Isolation : 402.930389,0.001538,0.955803
    Isolation : 402.859711,0.000516,0.320589
    Isolation : 402.794983,-0.001248,-0.775677
    Isolation : 402.826019,-0.000735,-0.456579
    Isolation : 402.893524,0.001756,1.091495
    Isolation : 402.928406,0.001074,0.667571
    Isolation : 402.833405,-0.001375,-0.854408
    Isolation : 402.805511,-0.000980,-0.609269
    Isolation : 402.902618,0.002127,1.322319
    Isolation : 402.899841,0.000993,0.617023
    Isolation : 402.810364,-0.000634,-0.393803
    Isolation : 402.788788,-0.000289,-0.179679
    Isolation : 402.888672,0.001623,1.008887
    Isolation : 402.782227,0.000658,0.409161
    Isolation : 402.811951,-0.001170,-0.727514
    Isolation : 402.884705,-0.000946,-0.588095
    Isolation : 402.843262,0.001056,0.656388
    Isolation : 402.789185,0.000516,0.320440
    Isolation : 402.746033,-0.000872,-0.542020
    Isolation : 402.841827,-0.000746,-0.463438
    Isolation : 402.839447,0.001486,0.923744
    Isolation : 402.808014,0.000918,0.570351
    Isolation : 402.807739,-0.000786,-0.488787
    Isolation : 402.873657,-0.000806,-0.500865
    Isolation : 402.861694,0.001251,0.777914
    Isolation : 402.817627,0.001036,0.643863
    Isolation : 402.869995,-0.000708,-0.440326
    Isolation : 402.834839,-0.000534,-0.331922
    Isolation : 402.849976,0.001391,0.864696
    Isolation : 402.846954,0.001021,0.634469
    Isolation : 402.834991,-0.000932,-0.579447
    Isolation : 402.820648,-0.000712,-0.442861
    Isolation : 402.825775,0.001489,0.925832
    Isolation : 402.862335,0.000783,0.486401
    Isolation : 402.803284,-0.000525,-0.326256
    Isolation : 402.812225,-0.000443,-0.275259
    Isolation : 402.891693,0.001290,0.801771
    Isolation : 402.854858,0.000465,0.288829
    Isolation : 402.817230,-0.000791,-0.491620
    Isolation : 402.795380,-0.000638,-0.396636
    Isolation : 402.889465,0.001041,0.646994
    Isolation : 402.845764,0.000548,0.340421
    Isolation : 402.814178,-0.000893,-0.554843
    Isolation : 402.932098,-0.000141,-0.087677
    Isolation : 402.879852,0.001023,0.636109
    Isolation : 402.818268,0.000724,0.449869
    Isolation : 402.858398,-0.001062,-0.660116
    Isolation : 402.810516,-0.000982,-0.610163
    Isolation : 402.797882,0.000627,0.389926
    Isolation : 402.806946,0.001061,0.659519
    Isolation : 402.850372,-0.001137,-0.706788
    Isolation : 402.788666,-0.001077,-0.669659
    Isolation : 402.892609,0.001116,0.693666
    Isolation : 402.837097,0.000931,0.578701
    Isolation : 402.810913,-0.000551,-0.342360
    Isolation : 402.872223,-0.001062,-0.659967
    Isolation : 402.856018,0.000712,0.442264
    Isolation : 402.751556,0.000542,0.336693
    Isolation : 402.763153,-0.000458,-0.284803
    Isolation : 402.878662,-0.000834,-0.518162
    Isolation : 402.901703,0.001186,0.737355
    Isolation : 402.837341,0.000907,0.563492
    Isolation : 402.785767,-0.000535,-0.332816
    Isolation : 402.735229,-0.000948,-0.589437
    Isolation : 402.871307,0.001426,0.886168
    Isolation : 402.837738,0.001362,0.846654
    
    -----------VP-----------------------------
    vdc, VinADC, VN
    
    Isolation : 402.869049,-0.582783,-362.251129
    Isolation : 402.903656,-0.505689,-314.330193
    Isolation : 402.928131,-0.446595,-277.598427
    Isolation : 403.011047,-0.390590,-242.786440
    Isolation : 402.997467,-0.344344,-214.040466
    Isolation : 402.912231,-0.298031,-185.252904
    Isolation : 402.860229,-0.262949,-163.446108
    Isolation : 402.816681,-0.230264,-143.129547
    Isolation : 402.714203,-0.204016,-126.814237
    Isolation : 402.837616,-0.176194,-109.520161
    Isolation : 402.885895,-0.155262,-96.509310
    Isolation : 402.950897,-0.136580,-84.896664
    Isolation : 402.918671,-0.120750,-75.056514
    Isolation : 402.868652,-0.103565,-64.374927
    Isolation : 402.776154,-0.091231,-56.708369
    Isolation : 402.784454,-0.081579,-50.708577
    Isolation : 402.871948,-0.072465,-45.043394
    Isolation : 402.885651,-0.061212,-38.048880
    Isolation : 402.820770,-0.053919,-33.515299
    Isolation : 402.780762,-0.048617,-30.219493
    Isolation : 402.897614,-0.042682,-26.530480
    Isolation : 402.875244,-0.036342,-22.589616
    Isolation : 402.853668,-0.031861,-19.804218
    Isolation : 402.834717,-0.029176,-18.135364
    Isolation : 402.903137,-0.025649,-15.942981
    Isolation : 402.851562,-0.021320,-13.252267
    Isolation : 402.809845,-0.018797,-11.684063
    Isolation : 402.812622,-0.017608,-10.944620
    Isolation : 402.880890,-0.015532,-9.654509
    Isolation : 402.958282,-0.012253,-7.616605
    Isolation : 402.875244,-0.010452,-6.496928
    Isolation : 402.794312,-0.010457,-6.500209
    Isolation : 402.849579,-0.009996,-6.213319
    Isolation : 402.974182,-0.007318,-4.548491
    Isolation : 402.873016,-0.006108,-3.796374
    Isolation : 402.813934,-0.006599,-4.101605
    Isolation : 402.771423,-0.006400,-3.978439
    Isolation : 402.900909,-0.004040,-2.511183
    Isolation : 402.863281,-0.003383,-2.103066
    Isolation : 402.799469,-0.004189,-2.604080
    Isolation : 402.867096,-0.004372,-2.717404
    Isolation : 402.863678,-0.002141,-1.330669
    Isolation : 402.812225,-0.001332,-0.828164
    Isolation : 402.905243,-0.002641,-1.641715
    Isolation : 402.885101,-0.002619,-1.628146
    Isolation : 402.848541,-0.000621,-0.386198
    Isolation : 402.783539,-0.000197,-0.122271
    Isolation : 402.886963,-0.001734,-1.077627
    Isolation : 402.932220,-0.001989,-1.236580
    Isolation : 402.884857,-0.000190,-0.118394
    Isolation : 402.789581,0.000168,0.104378
    Isolation : 402.832214,-0.001253,-0.778808
    Isolation : 402.896942,-0.002081,-1.293540
    Isolation : 402.919067,0.000048,0.029673
    Isolation : 402.797211,0.000193,0.119736
    Isolation : 402.748413,-0.000773,-0.480287
    Isolation : 402.862213,-0.001809,-1.124747
    Isolation : 402.960632,0.000027,0.016850
    Isolation : 402.869598,0.000527,0.327747
    Isolation : 402.804199,-0.000718,-0.445992
    Isolation : 402.860229,-0.001019,-0.633127
    Isolation : 402.864838,0.000352,0.218895
    Isolation : 402.804047,0.000823,0.511452
    Isolation : 402.850891,-0.001056,-0.656388
    Isolation : 402.913147,-0.001552,-0.964601
    Isolation : 402.851959,0.000432,0.268251
    Isolation : 402.861298,0.000968,0.601962
    Isolation : 402.799591,-0.000730,-0.453597
    Isolation : 402.844452,-0.000807,-0.501909
    Isolation : 402.935120,0.000251,0.155821
    Isolation : 402.837219,0.000967,0.601217
    Isolation : 402.900238,-0.000802,-0.498479
    Isolation : 402.854187,-0.001048,-0.651169
    Isolation : 402.921570,0.000428,0.266164
    Isolation : 402.863281,0.001091,0.677860
    Isolation : 402.841431,-0.000722,-0.448527
    Isolation : 402.872223,-0.000633,-0.393206
    Isolation : 402.816956,0.000335,0.208308
    Isolation : 402.854309,0.000558,0.346833
    Isolation : 402.867615,-0.000832,-0.517267
    Isolation : 402.812622,-0.000976,-0.606585
    Isolation : 402.865387,0.000644,0.400066
    Isolation : 402.817230,0.000934,0.580490
    Isolation : 402.834991,-0.000516,-0.320888
    Isolation : 402.794464,-0.000688,-0.427800
    Isolation : 402.861816,0.000105,0.065460
    Isolation : 402.881042,0.000237,0.147620
    Isolation : 402.797485,-0.000878,-0.545896
    Isolation : 402.858276,-0.001143,-0.710366
    Isolation : 402.900116,0.000609,0.378444
    Isolation : 402.829987,0.001154,0.717225
    Isolation : 402.827362,-0.000391,-0.242902
    Isolation : 402.880768,-0.001185,-0.736759
    Isolation : 402.817627,0.000854,0.530687
    Isolation : 402.887482,0.001161,0.721400
    Isolation : 402.798126,0.000082,0.050698
    Isolation : 402.838806,-0.000839,-0.521591
    Isolation : 402.821289,0.000708,0.440326
    Isolation : 402.852478,0.001126,0.700078
    Isolation : 402.887756,-0.000404,-0.251402
    Isolation : 402.864990,-0.001283,-0.797447
    Isolation : 402.858917,0.000116,0.072170
    Isolation : 402.872101,0.001249,0.776124
    Isolation : 402.816040,0.000105,0.065013
    Isolation : 402.809845,-0.000879,-0.546195
    Isolation : 402.797363,0.000123,0.076494
    Isolation : 402.826294,0.001094,0.680246
    Isolation : 402.854706,0.000100,0.061881
    Isolation : 402.850647,-0.000830,-0.515925
    Isolation : 402.797089,0.000294,0.182661
    Isolation : 402.846161,0.001164,0.723786
    Isolation : 402.813934,-0.000540,-0.335351
    Isolation : 402.778137,-0.001393,-0.865740
    Isolation : 402.878662,-0.000081,-0.050251
    Isolation : 402.897339,0.000560,0.348175
    Isolation : 402.801025,-0.000454,-0.282119
    Isolation : 402.786285,-0.001356,-0.842926
    Isolation : 402.801575,0.000439,0.273172
    Isolation : 402.856812,0.001323,0.822647
    Isolation : 402.880890,0.000281,0.174609
    Isolation : 402.861694,-0.000755,-0.469253
    Isolation : 402.836426,0.000298,0.185047
    Isolation : 402.767212,0.001143,0.710217
    Isolation : 402.874176,0.000036,0.022665
    Isolation : 402.885101,-0.001468,-0.912412
    Isolation : 402.865631,-0.000211,-0.131069
    Isolation : 402.803528,0.000748,0.465227
    Isolation : 402.748810,0.000063,0.039067
    Isolation : 402.887482,-0.000417,-0.259454
    Isolation : 402.944580,0.000127,0.078731
    Isolation : 402.895508,0.000458,0.284803
    Isolation : 402.831299,-0.000075,-0.046821
    Isolation : 402.844330,-0.000766,-0.476112
    Isolation : 402.928925,0.000071,0.044435
    Isolation : 402.883392,0.000545,0.338632
    Isolation : 402.810760,-0.000242,-0.150304
    Isolation : 402.849579,-0.000788,-0.489682
    Isolation : 402.853149,-0.000275,-0.171180
    Isolation : 402.893005,0.001193,0.741381
    Isolation : 402.856964,-0.000232,-0.144191
    Isolation : 402.841553,-0.000564,-0.350561
    Isolation : 402.778412,0.000067,0.041751
    Isolation : 402.818146,0.001242,0.771800
    Isolation : 402.894318,-0.000040,-0.024902
    Isolation : 402.847076,-0.000884,-0.549326
    Isolation : 402.793549,0.000350,0.217852
    Isolation : 402.862213,0.001236,0.768072
    Isolation : 402.835510,0.000407,0.252744
    Isolation : 402.866699,-0.001337,-0.831295
    Isolation : 402.861694,0.000029,0.017744
    Isolation : 402.822205,0.001246,0.774633
    Isolation : 402.837219,0.000218,0.135244
    Isolation : 402.819458,-0.000924,-0.574377
    Isolation : 402.901306,-0.000366,-0.227395
    Isolation : 402.872467,0.000774,0.481331
    Isolation : 402.781036,0.000258,0.160295
    Isolation : 402.830780,-0.001408,-0.875432
    Isolation : 402.928528,-0.000270,-0.167899
    Isolation : 402.876831,0.001129,0.701718
    Isolation : 402.852997,0.000701,0.435852
    Isolation : 402.865631,-0.001126,-0.699630
    Isolation : 402.865906,-0.000363,-0.225456
    Isolation : 402.803284,0.001361,0.845908
    Isolation : 402.828003,0.000422,0.262436
    Isolation : 402.886566,-0.001280,-0.795509
    Isolation : 402.850372,-0.000715,-0.444352
    Isolation : 402.809967,0.000829,0.515180
    Isolation : 402.773926,0.000793,0.493111
    Isolation : 402.835632,-0.001139,-0.707831
    Isolation : 402.898132,-0.000394,-0.244841
    Isolation : 402.799316,0.001053,0.654449
    Isolation : 402.789459,0.000588,0.365770
    Isolation : 402.903015,-0.001312,-0.815341
    Isolation : 402.935760,-0.000915,-0.568860
    Isolation : 402.871033,0.000562,0.349368
    Isolation : 402.782745,0.000390,0.242157
    Isolation : 402.772736,-0.001013,-0.629548
    Isolation : 402.936951,-0.000769,-0.477753
    Isolation : 402.926422,0.001097,0.681886
    Isolation : 402.816833,0.000657,0.408565
    Isolation : 402.797485,-0.000729,-0.453298
    Isolation : 402.889709,-0.000511,-0.317458
    Isolation : 402.936432,0.000398,0.247674
    Isolation : 402.889984,0.000507,0.315370
    Isolation : 402.875366,-0.000293,-0.182214
    Isolation : 402.803009,0.000179,0.111386
    Isolation : 402.798126,0.000551,0.342658
    Isolation : 402.799469,-0.000240,-0.149410
    Isolation : 402.873657,-0.000335,-0.208159
    Isolation : 402.934570,-0.000183,-0.113772
    Isolation : 402.883545,0.000747,0.464333
    Isolation : 402.804321,0.000164,0.101843
    Isolation : 402.768280,-0.000212,-0.131516
    Isolation : 402.825897,-0.000330,-0.204879
    Isolation : 402.921417,0.000831,0.516671
    Isolation : 402.888519,0.000230,0.142849
    Isolation : 402.822357,-0.000763,-0.474174
    Isolation : 402.831177,-0.000246,-0.152988
    Isolation : 402.763397,0.000776,0.482077
    Isolation : 402.753662,0.000923,0.573780
    
    
    Vdc: 402.811035, Vp: 0.193206, Vn: -0.100364, RisoP: 1465843947.595337, RisoN: 761453281.076513 
    

  • Hi Andreas ,

    Any update on the issue why the Vin ADC & VP values are decreasing over time after the switch is Turned ON ? I have also shared the log from our Firmware.

    This would cause problem as we are having a wide range of data whose value is decreasing constantly with time, and we need to take average of 20 value from them to further calculate RisoP & RisoN .

    Also request you to kindly share your email , so we can connect as this task of isolation monitoring is on priority.

    Regards,

    Kanhaiya

  • 0638.Isolation Monitering Updated.TSC

    Hi Kanhaiya,


    Find the updated simulation below.
    For  loss of PE detection you still need R_PE_N and R_PE_P but you also need some RisoP and RisoN in the simulation, otherwise there will be no closed loop.
    The connection towards PE for R_PE_P and R_PE_N also needs to be a seperate connection to PE than the connection of RinAMC,
    Also, you can never turn on SP and SN and at the same time, The results will not make sense.
    The procedure is to turn on SP-> Measure VP -> turn off SP -> turn on SN -> Measure VN -> Turn of SN -> Calculate RisoP/N
    The same is true if loss of PE detection is enabled. Just the calculation for RisoP and RisoN is different then.

    Constantly decreasing voltages can appear if you keep measuring the voltage after the Switch is turned off, since the sampling capacitor of the ADC needs to be constantly recharged. Only do measurements while the switches are in the right configuration.


    Best regards,
    Andreas

  • Hi Andreas,

    Thanks for the updated Simulation

    The Constantly decreasing voltages appear even when the Switch is turned On. 

    As you can see , even we have the kept the switch ON. The VinADC kept on decreasing with time.

    What could be the reason for this effect , we are unsure about which of the 20 sample should be considered out of these decreasing values ?

    Also should these value be stable or this effect will be seen?

    We are following the procedure is to turn on SP-> Measure VP -> turn off SP -> turn on SN -> Measure VN -> Turn of SN -> Calculate Riso P/N.

    but for Measurement of VP,VN we are taking 100 sample each, (The samples i had sent you earlier you can verify)

    The behavior of VinADC kept on decreasing with time is observed when switch is Turned on and 200 samples(100 Sample VP & 100 Sample VN) are collected.

    Regards,

    Kanhaiya

  • Hi Andreas,

    For isolation Monitoring , now we are applying 1.245 Mega ohm from Earth to DC- & Earth to DC+ using the addictional switches . Then we are calculating RisoP & RisoN which we are getting close to 1.245 Mega Ohm. which is nothing but (RisoN || RPE) &  (RisoP || RPE). 

    Then we used it in the Eq 21 & 22 to obtain the Actual RisoP & RisoN values. 

    then We keep a threshold at these Actual RisoP & RisoN value for warning and fault.

    lets suppose that the actual RisoP & RisoN value drops to 500k , we would then get value (1.245Mohm || 500k)  then we can find out Actual RisoP & RisoN 

    Using Equation 21 & 22 which would be 500k and then we could issue warning.

    We are using this approach because by just using 2 switches , we were getting very high unstable Actual RisoP & RisoN Values.

    Can we use this approach for isolation monitoring  ???

  • Hello Andreas 

    Any update regarding the issue ? can we use this method ?

    Regards 

    Kanhaiya 

  • Hi Kanhaiya,

    I am sorry about the issues you are facing. In our labs we did not face any of this issues.


    Regarding the constantly decreasing voltage:

    1. Is this the voltage at the input of the ADC? If yes, is the voltage at the input of AMC3330 also decreasing? 

    2. Is this voltage decreasing to 0 or is it settling ta value greater than 0.
    If it is settling to a value greater than 0 it can be caused by a capacitor which is discharging. In that case you need to wait with the measurement until the voltage is settled.


    Yes, you can use the procedure you are describing above, If equation 21 or 22 is leading to a value below 500k, you can issue a warning.
    The threshold should be set for the actual RisoP/N values.

    Best regards,

    Andreas

  • Hello Andreas,

    Thanks for the confirmation on the procedure. 

    In the design guide , i see there is a Test setup where in place of  RisoN & RisoP ,Resistor Bank are used .

    And the set value of resistor bank will appear on Finding RisoP & RisoN.

    Question is , have you guys removed those resistor bank and got a stable RisoP & RisoN Values ?

    Like some stable value of RisoN & RisoP in Mohm ??

    Regards,

    Kanhaiya

  • Hi Andreas ,

    Any update regarding the above case??

    Regards

    Kanhaiya

  • Hi Kanhaiya,

    We only tested with a resistor bank, simulating RisoP and RisoN. When these resistor banks are removed you are simulating RisoP and RisoN going towards infinite, which will lead to unstable results, since the result is only dependent on noise at this point.

    Best regards,

    Andreas