I'm looking for a pspice model of voltage regulator LP2953. I suppose it's difficult to find, so... Anyone can provide me with a reliable home made model or any advice to create a simplified one?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Florencio,
If you are using PSpice verison 15.7 or higher, you could use the LP2951 PSpice model that is in the product folder. The devices are very similar except for output current limit and a different shutdown function (the LP2952/53 is a quicker shutdown).
Please note that the model is in the LP2951-N product folder.
Britt
Thank you very much, you have moved me to check the Pspice versions. At the office I have the 16 one and I have not asked the team to update it yet, it includes the LP2951 (I think in OPAMP folder); nevertheless, at home I have the 16.5 one (which I use with less frequency), and here there is a folder of regulators, even with the LP2953. So no problem...
Thanks.