Hi,
The CSD16323Q3 is listed as having a breakdown voltage of 60V when in reality it is only 25V. This error causes the part to be recommended in simulations where the input voltage is greater than 25V. If the part is actually used in this manner, then it will likely fail and cause a system failure. Please correct this issue. Thanks.
Jatan Naik