Hi All,
I am designing `` Input Current Regulated Boost Converter` in Current Mode with DCR sensing method. To control switching, i am using TPS43061 as external controller.
TPS43061 has Tina Spice reference model which uses FB pin of the device to regulate ouput voltage. In my application I want use external error amplifier, that is why I have cancelled the FB and SS pin of the device and connect the error amplifier output directly to the compensation pin of the TPS43061 TINA model.
But unfortunatelly comp pin is not reacting to any change and model is still try to regulate inductor current to some numbers eventhough comp pin is floating ( FB and SS pin is connected to the ground) .
I have added my circuit schematic to the post. As you will see, Average input current is sensed with rsense, amplified and sended as input for error amplifier. Error amplifier has external reference voltage which can direct whole regulation to drive the expected inductor current. At the end system should be stable when expected inductor current is settled down.
In this simulation output voltage will be maximum 10v and will be controlled by power supply.
can you please inform me why tina model is not supporting my simulation? Why comp pin is not reacting properly ?
Thanks and Regards
Canan Simsek