This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2700 Compensation- no solutions

Other Parts Discussed in Thread: TPS55340, LM2700

HI

Since 2 days i would like to find the compensations value (Rc, Cc and Cc2) for the LM2700. I'm getting completely different results if i try Instructions from the PDF Manual, the slva636.pdf Dokument or the TPS55340_BOOST_CALCTOOL_REVC.xls Tool). I'm lost and would like to find the optimum values without much try and error.

I think it should be a type II compensation for this current-mode PWM controller....

Somebody can calculate and/or simulate the best values for me? Thank you very much

Andy

All the given components:

  MIN TYP MAX    
Vout     17.5 V Output Voltage
Vin 2.2   12 V Input voltage
Ilim 2.55 3.6 4.3 A Switch current limit
fsw 1 1350 1500 kHz Switching frequency
gea   155 290 µMhos Transconductance of error amplifier
Rea   0.85   Output resistance of error amplifier
Vref   1.26   V Reference voltage
Rdson   0.06   Ω Rdson of switch
Dmax 78     % Maximum duty cycle
Tonmin   ???200????   ns Minimum on time (estimate, not sure)
Vin_min, Vin_nom, Vin_max 4.8 5 5.3 V Minimum, nominal, and maximum input voltage
Vout     12 V Output voltage
Vripple     0.06 V Output voltage ripple (0.5% default)
fsw     1350 kHz Switching frequency
Kind     0.35   Inductor current ripple fraction (typical values 0.2 to 0.4)
eff_est     0.9   Estimated efficiency based on a similar design
IoutMin     0.2 A Minimum output current
Iout     0.5 A Output current
L     2.2 µH Chosen inductance
DCR     0.025 Ω DC resistance (DCR)
Cin     10 µF Input capacitance with derating
ESR     0.006 Ω Input capacitor ESR
Vd     0.24 V Forward voltage drop of output diode
Vinripple     0.011 V Input voltage ripple