This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Our customer observed Bode plot is different widely between SwitcherPro and EVM measurement result with Vout is 1V condition.
When EVM is defauly setting (Vout is 3.3V), the difference of Bode plot is small.
They modified EVM component value for 1Vout setting. Please refer to the attached file about component value.
The actual measurement result of that EVM is different from SwitcherPro result widely. We think actual measurement result with 1Vout condition is different from WEBENCH result too.
We would like to know the reason why the only 1Vout setting result is different from simulation widely.
Is there possibility that simulation model is not match with actual device at low output voltage condition?
Then phase curve drops suddenly at Gain is 0dB point in actual Bode plot. Do you have any opinion about this cause?
Best Regards,
Kohei Sasaki
.
John-san,
What influence would be removed by adding electrolytic capacitor to the input?
We can measure the bode plot with default EVM without any problem.
The bode plot of 1V output is the same as their customer board.
Best Regards,
Kohei Sasaki
John-san
I checked again with electrolytic capacitor at the input to the EVM. However it was not improve.
Then it was improve by changing comp components value.
Best Regards,
Kohei Sasaki
John-san,
Yes. I adjusted to Fco becomes low.
Then does the gain and phase curve change steeply depend on comp component value?
Best Regards,
Kohei Sasaki
John-san,
Please refer to the attached file P.1.
The bode plot Gain and Phase curve of this TPS54620 circuit has rapid change as point 1 and 2. What is the possible cause about this?
You said adding input bulk capacitor, however it didn't improve though I add a 220uF electrolytic capacitor.
The bode plot improved by changing compensation components value as P.2. Thus I think this relates to compensation circuit.
Could you give me your opinion about rapid change of Gain and Phase curve on attached file P.1?
20151125 TPS54620EVM measurement.pptx
Best Regards,
Kohei Sasaki