Other Parts Discussed in Thread: TPS54360, TINA-TI
Tool/software: Webench
Hi,
I am having issues running a load transient simulation after adjusting the compensation on the TPS54540-Q1 device using webbench. After running the Re-Comp tool and applying the changes to the circuit ,which only updates the values on the COMP pin, i am unable to run load transient simulations but all other simulations run just fine. What can i check to get this working again? or can it be a limitation of the tool?
Thank you,
Julio Sanchez
Fail Message:
Your simulation failed due to a convergence problem in the simulation netlist. If you recently changed a component in the BOM or changed a simulation related parameter, try changing it back to its previous value. If the problem persists, it may be due to an internal problem in our system. The problem has been logged and the development team has been notified. If you have any questions, please submit a feedback online at webench.ti.com/.../.
Error File Contents:
Simulation: FAIL
* ERROR * Transient analysis failed due to convergence problems. The transient parameter cmin=<value> could be helpful; it smooths abrupt transitions by adding the given capacitance to ground for every node. (SOLVER-12)
* ERROR * Transient analysis failed due to convergence problems. The transient parameter cmin=<value> could be helpful; it smooths abrupt transitions by adding the given capacitance to ground for every node. (SOLVER-12)
**************** ERROR/WARNING COUNT ****************
ERROR: Signals not found...pun2xxx conversion not done.Exit
* WARNING * TNOM is not defined on diode model main_block.d1.wb_diode. (DEVICE-23)
* WARNING * TNOM is not defined on diode model main_block.u1.wb_tps54360.d_d1. (DEVICE-23)
* WARNING * Device x_main_block.x_u1.r_r1 is shorted to 0 and will be removed. (EXPANDER-28)
* WARNING * Device x_main_block.x_u1.rpwrpd_0 is shorted to 0 and will be removed. (EXPANDER-28)
* WARNING * Device x_main_block.x_u1.rpwrpd_1 is shorted to 0 and will be removed. (EXPANDER-28)
* WARNING * TNOM is not defined on diode model main_block.u1.wb_tps54360.d_d.main_block.u1.wb_tps54360.dd. (DEVICE-23)
* WARNING * RS is not defined or equal to zero on diode model main_block.u1.wb_tps54360.d_d.main_block.u1.wb_tps54360.dd (DIODE-2)
* WARNING * Resistor x_input_block.x_vin.rsource has zero value. (RESISTOR-20)
* WARNING * Following dangling devices will be removed: x_main_block.x_u1.v_v47 (TOPOLOGY-50)
* WARNING * Following net will be removed after pruning dangling devices: x_main_block.x_u1.set0 (TOPOLOGY-51)
* WARNING * TIspice could not achieve requested tolerance at 270402 ns. (SOLVER-7)
* WARNING * TIspice could not achieve requested tolerance at 270402 ns. (SOLVER-7)
* WARNING * TIspice could not achieve requested tolerance at 270402 ns. (SOLVER-7)
* WARNING * TIspice could not achieve requested tolerance at 270402 ns. (SOLVER-7)
* WARNING * TIspice could not achieve requested tolerance at 270402 ns. (SOLVER-7)
* WARNING * Required transient step is limited by TMIN(1e-15) at time 270402 ns. (TRAN-20)
* WARNING * TIspice could not achieve requested tolerance at 270402 ns. (SOLVER-7)
* WARNING * Required transient step is limited by TMIN(1e-15) at time 270402 ns. (TRAN-20)
* WARNING * TIspice could not achieve requested tolerance at 270402 ns. (SOLVER-7)
**************** ERROR/WARNING COUNT ****************
Type: DEVICE #errors: 0 #warnings: 3
Type: DIODE #errors: 0 #warnings: 1
Type: EXPANDER #errors: 0 #warnings: 3
Type: RESISTOR #errors: 0 #warnings: 1
Type: SOLVER #errors: 2 #warnings: 7
Type: TOPOLOGY #errors: 0 #warnings: 2
Type: TRAN #errors: 0 #warnings: 2
--TOTAL-- #errors: 2 #warnings: 19
FAILED SIMULATION
Status = Fail