Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hello,
I am currently simulating a design that includes the PSpice model for the INA286, downloaded from the TI website. When I attempt to run the simulation, I get the following error (U2 references the INA286):
**** EXPANSION OF SUBCIRCUIT X_U2.XU1.XControl.XClkF1 ****
.PARAM TR_TM { IF (TR_MODE > 0.5, 1, 1000000 ) }
X_U2.XU1.XControl.XClkF1.VCLKF1 X_U2.XU1.XControl.46
+ X_U2.XU1.XControl.XClkF1.3 DC 0 AC 0 0 PWL 0 0 100N 0 REPEAT
+ FOREVER 0 0 1N -1 {2.015U*TR_TM}
--------------------$
ERROR(ORPSIM-16352): Time value must not be an expression
**** EXPANSION OF SUBCIRCUIT X_U2.XU1.XControl.XClkF32 ****
.PARAM TR_TM { IF (TR_MODE > 0.5, 1, 1000000 ) }
X_U2.XU1.XControl.XClkF32.VCLKF32 X_U2.XU1.XControl.ClkF3
+ X_U2.XU1.Startup DC 0 AC 0 0 PWL 0 0 125N 0 REPEAT FOREVER 0 0 1N 1 {50N*TR_TM}
----------------------------------------------------------------------$
ERROR(ORPSIM-16352): Time value must not be an expression
**** EXPANSION OF SUBCIRCUIT X_U2.XU1.XControl.XClkF2 ****
.PARAM TR_TM { IF (TR_MODE > 0.5, 1, 1000000 ) }
X_U2.XU1.XControl.XClkF2.VCLKF2 X_U2.XU1.XControl.48 0 DC 0 AC 0 0
+ PWL 0 0 125N 0 REPEAT FOREVER 0 0 1N 1 {1.965U*TR_TM}
-----------------------------------------$
ERROR(ORPSIM-16352): Time value must not be an expression
I have attached the relevant simulation file (.lib). What can I do to solve this?
ThanksINA286.lib