Other Parts Discussed in Thread: UCC28780
Hello,
Recently we have been working on module PMP40328, and we followed the BOM and PCB board on the web site (without changing any subjects). We faced some problems about the module. PMP40328 seems to be locked as we power it with Vac input = 100V at no-load and with load. The module seems to be locked out and we didn't know the reason. The Pin PWML and PWMH didn't output signals from UCC28780.
The signals below are some test results of our PMP40328 at Vac=100V input.
1. VDD (Triangle wave ranging from 10-17.5V)
2. VREF (REF output of UCC28780, which will drop to 0 )
3. Vgs of the Q7 (BSS126 H69006, ranging around -2V to -1.6V)
When problems appear in PMP40328, where should us check first?
We have measured the passive components and it seems OK. There is no voltage and current on the secondary side.
Thank you for answering the questions!
Sincerely,
Chiao