Part Number: TIDA-01541
Other Parts Discussed in Thread: AMC1311,
Hello,
I am trying to understand the input circuitry on the two AMC1311 parts (U12 and U15) used in TIDA-01541. In both cases, the SHTDN pin (pin 3) is connected to part of the input differential filter. I would expect that the SHTDN pin is connected directly to ground. Can you explain why the SHTDN pin is used in the input signal path?
Thanks in advance!