This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01541: Question on use of the AMC1311

Part Number: TIDA-01541
Other Parts Discussed in Thread: AMC1311,

Hello,

I am trying to understand the input circuitry on the two AMC1311 parts (U12 and U15) used in TIDA-01541. In both cases, the SHTDN pin (pin 3) is connected to part of the input differential filter. I would expect that the SHTDN pin is connected directly to ground. Can you explain why the SHTDN pin is used in the input signal path?

Thanks in advance!