This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Hi, Im trying to simulate some circuits using the NE5534, however when used as a unity gain buffer it needs an external compensation cap which is connected between pins 5 and 8, however in the default symbol of the opamp there is no pin 5 or 8. How do I connect a capacitors to this pins?
Thanks
Hi Jose,
When I open the file (the netlist text file), it says the following:
* CONNECTIONS: NON-INVERTING INPUT
* | INVERTING INPUT
* | | POSITIVE POWER SUPPLY
* | | | NEGATIVE POWER SUPPLY
* | | | | OUTPUT
* | | | | | COMPENSATION
* | | | | | / \
.SUBCKT NE5534 1 2 3 4 5 6 7
So, give pin 6 and 7 a try.
Herman