Other Parts Discussed in Thread: AMC1100, , DCH010505S
I am trying to build a current and voltage sensor for an inverter, using the mentioned TI design. In the design, power supply for the sensing circuit is designd with a transformer which is hard to find. All the solutions i found, had this transformer. I want a power supply design without a transformer. Can you please give me a design. It requires dual supply with +5V 0V -5V . I saw that there are some miniature 1W, 2W DC/DC isolated converters. Are there any way to use this miniature DC DC converters for powering the hot side of the AMC1100. Thank you