Other Parts Discussed in Thread: CC1310
Hey guys we are using TIDA 00489 layout and I have some questions regarding production.
- We want to use a CLI script to flash our software on the CC1310 andwe have to readout the MAC address of the chip for internal tracking of the device. I have not much experience and was wondering which options I should use. I basically want to use "erase", "programming" and "verify" functions. But there are several "detailed" options.
- What erase, CCFG and flash page options should I take?
- What reset and run actions should I use? (I think run after flashing should be correct)
- What else should I look for?
- How can I read out the MAC Address during/before/after this process automatically?
- We are thinking of using a SWD debugger for manual MAC read out via the JTAG header, can you recommend one we could buy? Because using JTAG cable, connect TIDA 00489 to Launchpad and readout MAC address of TIDA board using flashProgrammer does not work.
Hope I was clear about my issue.
Kind regards
Slev1n