This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools: How to set a Isolated DC DC converter with multiple isolated outputs in TI webench power architect

Other Parts Discussed in Thread: PMP40274, PMP4468, PMP11107

Tool/software: WEBENCH® Design Tools

Dear all,

I have a requirement of a DC DC converter with following specification

Input voltage 18V to 36V

Output1= 3.3V/7.5A

Output2= 1.5V/3A

Input to output isolation required and both outputs(3.3 and 1.5) should be isolated each other.

 I am facing problem in giving the isolation requirement. How to specify this isolation requirement in TI Webench power architecture?

Regards

Aneesh