This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS51120: Limiting the delay of MOSFETs used in the TPS51120

Part Number: TPS51120

Tool/software: WEBENCH® Design Tools

I have selected a MOSFET that is controlled by the TPS51120.

Are there any limitations on MOSFET delay parameters (rise time (tr), turn-on delay time (td (on)), fall time (tf), turn-off delay time (td (off))?

I am thinking of selecting FETs with the following parameters: Can I use (1) and (2) below?


(1) tr = 4.7ns, td (on) = 12ns, tf = 8.2ns, td (off) = 30ns
(2) tr = 4.6ns, td (on) = 15ns, tf = 11ns, td (off) = 67ns