This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hi,
I am doing load and input transient simulation for LMR16030 and getting an error message '"simulation failed".
Similarly, the input transient is also failed.
The parameter used in the simulation are: Input voltage: 18V to 47V, Output 15V, Output current 2.5A.
Please advise. Thanks.
Hi Deepti,
We have resolved the issue now. The changes will be moved to production in our next release.
Regards,
Atul