This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-00951
Hello,
C12 | 1 | 0.1uF | ECW-F6104JL | Panasonic | CAP, CERM, 100 pF, 50 V, +/- 1%, C0G/NP0, 0603 |
at the BOM file the part number is ECW-F6104JL, but this part number take me to 630V capacitor
which one is the correct one the 50v or the 630?
the same part number is mention in c8 as well
C8 | 1 | 0.1uF | ECW-F6104JL | Panasonic | CAP, Film, 0.1 µF, 1000 V, +/- 10%, TH |
which one is the correct one the1000v or the 630?
Thank you very much
Michael
Hi thank you
im adding another questions,
U1, U7 2TLP2361TLP2361(TPL,EToshibaIC, PhotocouplerSOP-4, is SOP 5 is also good?
and
U41FODM611FODM611FairchildIC, PhotocouplerSOP-4 , is Sop is also good?
Best Regards
Michael