This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00951: clarification about c12 at the BOM file

Part Number: TIDA-00951

Hello,

C12                                               1 0.1uF ECW-F6104JL Panasonic CAP, CERM, 100 pF, 50 V, +/- 1%, C0G/NP0, 0603

at the BOM file the part number is ECW-F6104JL, but this part number take me to 630V capacitor

which one is the correct one the 50v or the 630?

https://www.mouser.co.il/ProductDetail/Panasonic/ECW-F6104JL?qs=GoZnPdyRfjbMcIsYTsxlXg==

the same part number is mention in c8 as well

C8                     1 0.1uF ECW-F6104JL Panasonic CAP, Film, 0.1 µF, 1000 V, +/- 10%, TH

which one is the correct one the1000v or the 630?

Thank you very much

Michael