This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP40500: Will the 500W PMP40500 case be raised to 1000W, is the solution feasible, and are there any considerations for circuit design?

Part Number: PMP40500
Other Parts Discussed in Thread: LM5036

Hello.

I want to refer to your PMP40500 case (54V / 12V / 42A / 500W) case and make a (80V / 48V / 21A / 1000W) prototype.

I wonder if the solution is feasible?

What should be paid attention to in circuit design?

Thank you.