This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM2731: LM2731 efficiency calculation in WEBENCH

Part Number: LM2731


Tool/software: WEBENCH® Design Tools

Hi Team,

When simulating the LM2731 in WEBENCH, the working condition is: Vin= 4-8V, Vout=11V, Iout=30mA, the simulation result shows the efficiency is 91.9%.

However, if using LM27313, the simulation result shows efficiency is less than LM2731. It is only 75%. Why there is so big difference?