This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am facing convergence issue with the Pspice Model of UC3845 for 2-switch forward converter. The two freewheeling diodes, MOsfets and the UC3845 fail to converge. Can anybody guide me on what settings or changes must be done in order to debug this issue?
Hi Teng,
Please find the attached snapshot of the simulation schematic.
For this I have tried autoconvergence but still there is convergence error as below:
These devices failed to converge:
X_U115.G_Miller X_U115.G_Coss X_U125.XDRIVE.M1 X_U125.XDRIVE.M2 Q_Q6
Q_Q5
Last node voltages tried were:
NODE VOLTAGE NODE VOLTAGE NODE VOLTAGE NODE VOLTAGE
( D) 2883.2000 ( CS) 4127.0000 ( FB) 3.1089 ( DRV) 112.8E+03
( V18V) 12.1970 ( VGSL) 11.44E+03 ( VGSU) 798.7E+03 (VBULK) 325.0000
(N2075040) 70.60E+03 (N2075050) 1109.4000
(N2075056) 576.7700 (N2075074) 12.5060
(N2075542) 12.0040 (N2076336) 12.7830
(N2076356) 4.5646 (N2076452) 3.1095
(N2076480) 3.1089 (N2076484) 20.0000
(N2076628) 13.3690 (N2076698) 5.1060
(N2076714) 2108.4000 (N2076836) 13.5640
(N2076870) -1.2947 (N2076982) 4.5609
(N2078287) 1.017E+06 (N2078291) 1.015E+06
(N2078375) 797.8E+03 (N2078381) 791.4E+03
(N2078429)-786.9E+03 (N2078453) 112.8E+03
(N2078587)-377.5E+03 (N2078691) 229.8E+03
(N2078821) 227.3E+03 (N2078891) 10.53E+03
(X_U112.5) 1.017E+06 (X_U112.6) 1.017E+06
(X_U114.d) 9.999E+09 (X_U114.g) 5375.0000
(X_U114.s) 4127.3000 (X_U115.d) 10.00E+09
(X_U115.g) 792.6E+03 (X_U115.s) 791.4E+03
(X_U123.4) 3.1078 (X_U123.6) 12.7830
(X_U123.7)-7.970E-09 (X_U123.8)-17.12E-09
(X_U124.4) 7.0559 (X_U124.5) 1773.4000
(X_U124.6) 1774.8000 (X_U124.7) 1773.4000
(X_U125.5) 0.0000 (X_U125.6) 5.0000
(X_U125.7) 0.0000 (X_U125.8) 4.6418
(X_U125.9) 2.1089 (N20784690) 753.0E+03
(X_U112.20) 4127.0000 (X_U112.21) 4127.0000
(X_U114.aa) -79.9980 (X_U114.ba) -80.0010
(X_U114.d1)-786.9E+03 (X_U114.g2) 11.44E+03
(X_U114.ss) 4127.0000 (X_U114.sx) 4127.3000
(X_U114.Tj) 27.0000 (X_U115.aa) -79.9960
(X_U115.ba) -80.0010 (X_U115.d1) 325.0000
(X_U115.g2) 798.7E+03 (X_U115.ss) 791.4E+03
(X_U115.sx) 791.4E+03 (X_U115.Tj) 27.0000
(X_U125.10) 5.0000 (X_U125.11) .5468
(X_U125.12) 1.6405 (X_U125.13) 5.0000
(X_U125.16) .5468 (X_U125.19) 20.0000
(X_U125.21) 5.0000 (X_U125.22) 5.0025
(X_U125.50) 5.0000 (X_U125.51) 0.0000
(X_U114.d1k)-786.9E+03 (X_U114.d1z)-786.9E+03
(X_U115.d1k) 325.0000 (X_U115.d1z) 327.8800
(X_U125.150) 5.0000 (X_U125.191) 20.0000
(X_U114.11xy)-907.3E+03 (X_U114.Alfa) 2.000E-12
(X_U114.d1zd)-786.9E+03 (X_U114.Dev1) 9.999E+09
(X_U114.Dev2) .0569 (X_U114.Dev3) 0.0000
(X_U114.dfet)-907.3E+03 (X_U114.edep) 9.967E+09
(X_U115.11xy)-120.1E+03 (X_U115.Alfa) 2.000E-12
(X_U115.d1zd) 327.8800 (X_U115.Dev1) 9.999E+09
(X_U115.Dev2) -2.0068 (X_U115.Dev3) 0.0000
(X_U115.dfet)-120.1E+03 (X_U115.edep) 9.968E+09
(X_U114.11xxx) 4127.0000 (X_U114.Alfa2) 43.30E-12
(X_U114.Dev1c) 9.999E+09 (X_U114.Dev2c) .0569
(X_U114.Dev3c) 0.0000 (X_U114.Val_T)-5.400E-12
(X_U115.11xxx) 791.4E+03 (X_U115.Alfa2) 43.30E-12
(X_U115.Dev1c) 9.999E+09 (X_U115.Dev2c) -2.0068
(X_U115.Dev3c) 0.0000 (X_U115.Val_T)-5.400E-12
(X_U125.XAMP.2) 2.7521 (X_U125.XAMP.3) 2.9186
(X_U125.XAMP.5) 2.5281 (X_U125.XAMP.6) 2.5281
(X_U114.d_dedep) 9.998E+09 (X_U115.d_dedep) 9.999E+09
(X_U125.XAMP.10) 2.5530 (X_U125.XAMP.13) 2.3348
(X_U114.d1bvdss1)-786.9E+03 (X_U115.d1bvdss1) 325.0000
(X_U125.XDRIVE.2) 252.2700 (X_U125.XDRIVE.3) 252.2700
(X_U125.XLATCH.3) 5.0000 (X_U125.XLATCH.4) 5.233E-09
(X_U125.XLATCH.7) 43.12E-09 (X_U125.XLATCH.8) 5.0000
(X_U125.XLATCH.9) 0.0000 (X_U125.XLATCH.10) 5.0000
(X_U125.XToggle.3) 5.0000 (X_U125.XToggle.4) 5.0000
(X_U125.XToggle.7) 43.12E-09 (X_U125.XToggle.8) 5.0000
(X_U125.XToggle.9) 0.0000 (X_U125.XToggle.10) 5.0000
(X_U125.XLATCH.X1.5) 5.0000 (X_U125.XLATCH.X2.5) 0.0000
(X_U125.XLATCH.X3.5) 0.0000 (X_U125.XLATCH.X4.5) 5.0000
(X_U125.XLATCH.X5.5) 5.0000 (X_U125.XLATCH.X6.5) 0.0000
(X_U125.XLATCH.X7.3) 0.0000 (X_U125.XLATCH.X8.3) 5.0000
(X_U125.XToggle.X1.5) 5.0000 (X_U125.XToggle.X2.5) 0.0000
(X_U125.XToggle.X3.5) 0.0000 (X_U125.XToggle.X4.5) 5.0000
(X_U125.XToggle.X5.5) 5.0000 (X_U125.XToggle.X6.5) 0.0000
(X_U125.XToggle.X7.3) 5.0000 (X_U125.XToggle.X8.3) 5.0000
Request you to help me with this issue.