Tool/software: WEBENCH® Design Tools
Dear support, researchers,
i have a question,
I am using the following DC drivers from polulu,
one has a offset of 50mV and 10mV/A and the other roughly 140mV/A, the 140mV/A is for dc motors and an Electromagnet
the maximum current I have set for the Peltiers I am going to use is 20A. the max current possible is 15.7A at 25V.
12 bits ADC from the new Teensy4.1.
which op amp in single supply is best for such an easy application
I would like to create the maximum range for the input of the ADC possible.
20A =3.3V
0A=0V with 50mV offset.
200mV max input on the opamp +50mV offset.
so the total input voltage on the inverting opamp will be 0.25V with offset = gives me an 13.2 V amplification.
Best
Bastiaan