Other Parts Discussed in Thread: UCC21520, , UCC21750, ISO5852S, ISO5452
Hi TI Experts,
I am planning to replace my MOSFETs with SIC MOSFETs. I have seen TIDA-01605 reference design From TI. Currently i am using UCC21520 isolated dual channel driver.
My question is when i drive my MOSFETs there is no extra protection stage. But in TIDA-01605 there is short circuit detection circuit and two level turn off circuit.
What is the risk in removing these circuits?. Can i simply drive a SIC MOSFETs with +15V and -5V without these protection circuits?
Regards
Aneesh