Other Parts Discussed in Thread: CC3100MOD
Hello,
A customer of mine is going to manufacture the TIDA-00380 board.
They are asking the following:
In order to enable the SMA external antenna on the board, There are same missing components which are not assembled like: J6 – SMA connector,C17 and R13.
Which SMA antenna do you recommend?
In what components did TI test the SMA option?
*This question above is about the values of the components that are actually used to the RF matching to the SMA connector.