Tool/software: WEBENCH® Design Tools
Can the LMR50410 chip eliminate voltage fluctuations? What is the approximate range of the voltage that can be eliminated?Our input power supply may be affected by the yellow voltage fluctuations as shown in the figure below, but we used the L6984 chip before, which could not eliminate the output voltage fluctuations as shown in the blue line in the figure below. Can your chip eliminate this fluctuation and output a stable voltage? If not, please recommend a chip that can eliminate this fluctuation. Our requirements: input voltage 5-36V, output voltage 5V.