This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH Tools/UCC2813-3-Q1: soft start vs slope compensation

Part Number: UCC2813-3-Q1

Tool/software: WEBENCHRegistered Design Tools

Greetings

I am using UCC2813-3-Q1 for a simple forward converter. I find that the soft-start is not working. The first output pulse appears as COMP pin is around 1V. But the duty cycle is high. This IC comes with internal soft-start. I do not have anything external for soft-start. I also do not have any slope compensations since my application does not require above 45% duty. 

Is there a correlation between the slope compensation and the soft-start circuitry?


Thanks

Vijay