Hi Ti,
I have connect 4 tags to 1 anchor(coordinator) with RF cable(conductive test)
The default python script will send RTLS_CMD_CREATE_SYNC all(FF:FF:FF:FF:FF:FF)' 4 times, flow as below(I think it is just a workaround, will you use 1 command to establish sync all devices in adv list?)
==========================
CREATE_SYNC all
SyncRsp pass
RTLS_EVT_SYNC_EST TAG-A
CREATE_SYNC all
SyncRsp pass
RTLS_EVT_SYNC_EST TAG-B
CREATE_SYNC all
SyncRsp pass
RTLS_EVT_SYNC_EST TAG-C
CREATE_SYNC all
SyncRsp pass
RTLS_EVT_SYNC_EST TAG-D
==========================
It is easy to have a problem--> not receiving SYNC_EST of a certain tag
I try to enlarge sync_timeout value(5000) of CREATE_SYNC, looks like there is some improvement, and i can see the interval of CREATE_SYNC and RTLS_EVT_SYNC more than 4s for a certain tag(others are about 200ms)
so i guess sometimes a certain tag need more time to complete RTLS_EVT_SYNC_EST. but I still have a high probability of SYNC_EST fail even enlarge sync_timeout to 5s.
Do you have the same problem on muti tag and know why sometimes need so much time to establish sync?