Other Parts Discussed in Thread: TMP007,
Hi,
I'm trying to establish an i2C connection to an LSM9DS1 3-Axis motion Sensor. I started with trying to open an I2C Transfer with the TMP007 Example and the CC2650 as a Master Read. I can not see at least the CC2650 sending the Slave address over I2C Bus. I read in the datasheet from the LSM9DS1 that i need Pullup resistors for I2C connection.
I was looking in the Datasheet for the CC2650 but i could not find information about the value of the internal PullUps at DIO4 and 5 wether pullup is enabled in I2C mode or not.
Do i need external Pullup for I2C Transfers with the CC2650 and what value?
best regards
Kai