This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2650: How to generate bin file for simple ble peripheral project in CC2650?

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2640

Hello,

I am using LAUNCHXL-CC2650

BLE SDK 2_02_07_06

CCS7.4

Compiler TI v5.2.6.

I have successfully done OAD update using the simple ble peripheral example code. and I can update my BLE application over the air.

In process, by mistake I deleted the folder  "FlashOnly_OAD_ExtFlash".

So, Earlier I was able to see .bin file of the project. But now, I don't see any file with .bin being generated in that folder.

I have done Rebuild of project then also - No luck.

We are using this file for OAD update from android application.

I have also attached Images of post build setting.

do I need to change anything in post build settings?

Any solution?

Thank you

Dnyaneshvar Salve