Hi,
When the CC2340 is powered on multiple times, it has been found that the external 32.768kHz crystal oscillator sometimes fails to start oscillating. During debugging, it was discovered that the program does not enter the PowerCC23X0_oscillatorISR interrupt. What could possibly cause this issue? The crystal oscillator is connected to an external 15pF capacitor.
Normally, after a successful start of the 32.768kHz crystal oscillator, the code would enter this section, but when the issue occurs, it does not enter here.