Part Number: CC2652R7
Other Parts Discussed in Thread: ENERGYTRACE,
1) I have setup the device in periodic advertisement mode using the information in this thread - Link . While detecting it on a sniffer, I am receiving an error which indicates some issue with - Aux_Sync_Ind packet. How do I rectify this ? PFA the project I am using.
2) I want to calculate the energy consumption from these boards while working in periodic advertising mode. Currently the device is sending out ADV_EXT_IND and AUX_ADV_IND again and again after the specified advertising interval, I want to setup these boards such that when a scanner device has detected the periodic advertiser, it should stop sending out the above 2 indications and only AUX_SYNC_IND are sent after that. Basically I want the device to be registered with the scanner and just send out the sync packets after that. How do I achieve this?
3) How to control the time interval between AUX_SYN_IND packets?
1830.simple_peripheral_LP_CC2652R7_tirtos7.zip
Regards,
Garvit