Tool/software:
Can you please provide links for examples which helps with the below:
- CC2640R2F ADC Temperature Measurement Example
- CC2640R2F ADC Temperature Measurement Example
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Can you please provide links for examples which helps with the below:
- CC2640R2F ADC Temperature Measurement Example
- CC2640R2F ADC Temperature Measurement Example
Hello Shweta Savdekar,
I hope you are doing well. It does not seem we have a complete ADC temperature example like we do have on the cc13xx-cc26xx SDK, but I will keep on looking. We can reference the demo->portable->temperature to see how the CC2640R2 handles temperature.
If you also use BLE you can try the following:
In the driver lib we have a few functions that could be used (reference the text in the file, and TRM section 18):
Thanks,
Alex F
Hello Markel,
Thank you so much for the above information, it is helpful.
I am trying to read internal temperature sensor, do you any suggetions
Thank you Markel for sharing the above thread, can you help me with implementoing the periodic sampling
Hello Shweta Savdekar,
For periodic sampling reference adcsinglechannel example, and modify the ADC_SAMPLE_COUNT;. You could also setup a separate function or task with custom code for your specific case.
You can also modify the sampling duration if needed.
Thanks,
Alex F