Part Number: CC2340R5
Tool/software:
Dears,
- 1. When the customer CC2340R5 is in mass production, it needs to test the BLE physical layer parameters. Is there any way to let BLE enter different test modes through Bluetooth wireless signaling, such as
a) Emission test: power, modulation, frequency, spectrum;
b) Reception test: bit error rate, receiving sensitivity... - 2.It is mentioned in the application note that UART can be used The test command is configured, but the customer UART is occupied. The customer wants to use Bluetooth commands to configure the test options. Does your company's Bluetooth protocol stack have a method that can be configured in this way, such as the Bluetooth version of the HCI command
Thanks.