Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
Currently I am working on basic_ble Peripheral profile project. And we are facing an issue when trying to send data from module to mobile continuously with the size of MTU excahnged size 247(mtu_value) after multiple packets transmission from the module, we are getting an status as blePending.
After this error occurs we are not able to connect or pair with the module and module requires an power restart to recover.
Status = SimpleGattProfile_setParameter(SIMPLEGATTPROFILE_CHAR4, mtu_value,&uartReadBuffer[SentDataLen]);
And here are the interval settings calling SimpleGattProfile_setParameter() with 50 milliseconds and tried with 100,200 milliseconds and Connection interval parameters image attached below.
Kindly help us to resolve the issues.
SDK Version : simplelink_lowpower_f3_sdk_8_10_01_02 (peripheral)
CCS version: CCS 12.7.1
Regards,
Vignesh.