Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,team
SDK:C:\ti\simplelink_cc13xx_cc26xx_sdk_7_41_00_17.
code:
int bsp_uart_open(uint32_t baudrate, UART_FNCT_RESPONSE respfnct) { (void)baudrate; UART2_Params uartParams; /* Create a UART where the default read and write mode is BLOCKING */ UART2_Params_init(&uartParams); uartParams.readMode = UART2_Mode_NONBLOCKING; uartParams.writeMode = UART2_Mode_BLOCKING; uartParams.baudRate = UART_DEBUG_BAUDRATE; uart2_1_handle = UART2_open(CONFIG_UART_1_DEBUG, &uartParams); if (uart2_1_handle == NULL) { /* UART2_1_open() failed */ DEBUG_ASSERT(0); return -1; } /* Create a UART in CALLBACK read mode */ UART2_Params_init(&uartParams); uartParams.readMode = UART2_Mode_NONBLOCKING; uartParams.writeMode = UART2_Mode_BLOCKING; uartParams.baudRate = UART_MCU_BAUDRATE; uart2_0_handle = UART2_open(CONFIG_UART_0_BLE, &uartParams); if (uart2_0_handle == NULL) { /* UART2_0_open() failed */ DEBUG_ASSERT(0); return -1; } gBspUARTStat.respfnct = respfnct; gBspUARTStat.open_flag = true; return 0; }
After the previous task calls UART2_write, the next task calls this write interface function hardfault occurs.
error code: