This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-CC2652PSIP: LP-CC2652PSIP

Part Number: LP-CC2652PSIP

Tool/software:

Hello,

I tried to build and flash host_test project and was asked to update XDS110 of the LaunchPad board. 

Updater failed and board does not appear as USB device anymore, neither on Mac nor Windows machines...

How to restore the board?!

Mac OS 14.6.1 (23G93), 

CCS Version: 20.0.1.4__1.6.1

Error log:

IcePick_C: Warning: A firmware update is required for the XDS110 probe. The current firmware is version 3.0.0.18. The probe must be upgraded to firmware version 3.0.0.33 to be compatible with this software. Click the "Update" button to update the firmware. DO NOT UNPLUG THE DEBUG PROBE DURING THE UPDATE. (Emulation package 20.0.0.3283)
IcePick_C: Error: (Error -592 @ 0x0) The firmware updater encountered an error and could not finish. The firmware download failed to complete on the XDS110. Unplug and re-plug the XDS110, and try again. If the problem remains, try updating the firmware using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of the installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 20.0.0.3283)
IcePick_C: Error initializing emulator: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 20.0.0.3283)
IcePick_C: Error initializing emulator: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 20.0.0.3283)

Thank you in advance!