This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC256XQFNEM and DK-TM4C129X



I am using the CC256XQFNEM Eval module and the DK-TM4C129X eval board
The CC256xQFNEM board is supposed to work with Texas Instruments hardware development kit DK-TM4C129X

I wonder how the module is supposed to be attached to the board.
It fits into the EM connector, J19 and J31.
Because some jumpers, PB6 and PB7 protrude from the board the Bluetooth module does not fit in nicely, but remains a little bit tilted.

Is it correctly inserted?
Should it be turned 180 degrees?
Should something be done to the board, jumpers changed, or so.

Bluetooth does not work. HCI fails.
I compiled the SPPDemo, but it fails at BSC_Initialize() returning BTPS_ERROR_HCI_INITIALIZATION_ERROR.